Hello-
I need to design a motor and control system that simply moves (snaps may be a better description) a light weight arm back and forth between two positions (A ->B, B->A) quickly, traversing from A to B in less than 10ms (pretty fast I realize). Think of the arm as being something like a hand of a clock, where the hand is being snapped back and forth between 1 o’clock and three o’clock. There will be mechanical stops at 1 & 3 o’clock which will stop the motion of the arm at that position.
The angle between A and B is fairly flexible, but should be somewhere between 30 and 90 degrees. It would be preferable that while the motor is at each position (A or B), that it maintain some torque, pressing the hand of the clock up against the mechanical stop. I’ll be using one of the stops to open and close another circuit.
I also need the system to stay at each position for two seconds or so and then have it return, again quickly, to the other position. The pause between motions is not that critical. I’m a software developer, so I am very familiar with coding, however I know very little about hardware, motor controllers etc.
I’ve looked around at the various controllers but due to my inexperience in this sort of thing I was hoping that someone could point me in the right direction.
I greatly appreciate any suggestions!
Thanks,
Jim H