RTK EVK NTRIP Caster Through Ethernet

Hello,
I am attempting to configure an RTK EVK as an NTRIP Server (or NTRIP Caster by putting it into Base Caster mode in firmware v2.1). I would like to run NTRIP messages to my local ethernet switch, however, the rtk eth interface becomes unavailable for this service (un-ping-able with the set static IP through local network switch when directly plugged in and on the same subnet). There isn’t a lot of documentation on setting the NTRIP server up besides using rtk2go as the caster. Additionally, after putting the system into base caster mode, the serial interface will show the base NTRIP caster and TCP servers enabled but ‘waiting for network’; however both are unreachable through our rovers (this is after verifying multiple times that the mount points user/pw were correct). After working with v2.1 for awhile, I reverted to v1.4 and was able to ping the ethernet interface finally. However after enabling and setting up the NTRIP server, the serial interface reports that ‘NTRIP Server 0 state: NTRIP_SERVER_OFF.’ Please advise on if I am missing an additional setting or some other step, thanks.

Sorry cannot help but I’m curious about doing the same in the future. Hope it gets setup