RTK Facet_SW Maps NTRIP Client_Mount Points

Well, wiscors.dot.wi.gov:2101 returns this mount point table (filtered, removed everything with irrelevant CMR protocol):


All these are “smart” mount points that provide corrections based on the rover’s location (when the rover reports its location to the NTRIP caster correctly).
The “safest” mount point to try is SingleBase_RTCM31 because it simply acts as an automatic “switch” to send corrections directly from the nearest base station instead of doing any additional “magic.”
Otherwise, any failures to obtain a fixed solution are likely due to one of the factors:

  • The rover doesn’t recognize RTCM messages specific to a certain protocol.
  • The rover doesn’t send its location correctly so the caster can’t send proper data since it doesn’t know the rover’s location.

SW Maps absolutely allows typing in the mount point name by hand on Android, can’t say anything about iOS.

Another port, wiscors.dot.wi.gov:2102 returns a table of individual base stations.