SKU: GPS-17370
Product Name: SparkFun RTK Surveying Kit
UPC: 845156011780
I just received and began testing the RTK Surveyor and am unable to achieve a position fix, or even a single satellite. I charged the units internal battery, connected the supplied antenna (TOP106) to a tripod, and connected the antenna to the Surveyor. I set the switch to ‘Base’ mode and powered the unit. After not receiving a solid LED(BASE) indicating a successful survey-in in over 15 minutes, I connected the Surveyor to my laptop via USB-C (Config Ublox) The position of the antenna was ~5ft off the ground and in a position I have, regularly in the past, achieved a position-fix with the lesser neo-m8p. uCenter showed that the module was seeing no satellites. I repeated the above but in ‘Rover’ mode, but still could not get a single satellite. I’m not sure if I have a defective Surveyor or Antenna or Antenna Cable, or if it’s something else entirely. Any assistance in the matter would be really appreciated. Thanks in advance!