I’m trying to send NMEA via the config ublox port to an external device. The device needs to see a baudrate of either 19.2k or 38.4k and GGA at 10hz and GSA at 1hz. Can someone help me with these settings? I can connect to the interface via Wi-Fi but I find the message rate page confusing as it’s a send/fix rather then Hz. Also, the baudrate setting seems to be for the DATA port? Thanks
Ok so how do I ensure 10hz NMEA? If I set the fix hz to 2 and the message value to 5, I should be getting 10 messages/sec, correct? And that guide is still not clear on whether the baudrate is only for the DATA port or if it affects the usb port also.