RTKExpress/GPS Enclosure 3D Model

Does anyone know where I can find a 3d Model of the RTK Express enclosure? Or a holder for that it snaps into?

Hammond part # 1553BBK. I pushed this zip to the repos as well (I should have put these files there ages ago!).

A snap in holder is a fabulous idea! If you end up designing one, please share.

I’ve been working on one that incorporates the screen and a larger battery that has square edges and can be held by a smartphone clamp more easily.
It is still a bit rough, but I can share what I’ve done so far. I’ll post a link when I get the model posted.

Exactly, what I was looking for. Thank you !!!

Hi -

I made this clip that uses the existing enclosure’s screws to attach a pole snap clip. The dimensions are still a little loose (it slides a bit on the mono-pod) so I didn’t post it yet.

I tried to upload the stl, but the chat won’t let me (unsupported file type?)

If someone wants this I can adjust it a bit more and upload the stl (somewhere?). Its a jscad model and I can share that also.

Very nice! Don’t let perfect be the enemy of done. Grabcad is my goto for STL sharing.

I like that solution. Would a layer of electrical tape inside the clip give it enough grip?

Yes - I just haven’t put the tape on. Here is a link to the model and you can adjust the gap in the clip and the radius. The radius parameter is not quite the inner radius of the clip because I did not compensate for the 1.5mm wall thickness.

Print in this orientation so that the layers are perpendicular to the pole for strength. Supports are not necessary.

Github : GitHub - jbroll/jscad-models
Edit online : RTKClip.js