Hi there.
I’m using the RV1805 rtc with a 3.3v pro mini. Everything works great except the alarm/interrupt function. Currently I have example 4 from the library loaded and while the serial monitor is displaying the current time no problem I cannot get the alarm to trigger no matter if it’s set to seconds, minutes, hours ect…
Hello, have you checked your alarm circuit? Is it possible that there is anything wrong?
This is the sketch I am running:
/*
Getting the alarm to fire an interrupt on the RV-1805 Real Time Clock
By: Andy England
SparkFun Electronics
Date: 2/22/2017
License: This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).
Feel like supporting our work? Buy a board from SparkFun!
https://www.sparkfun.com/products/14642
This example shows how to set an alarm and make the RTC generate an interrupt when the clock time matches the alarm time
The INT pin will be 3.3V. When the real time matches the alarm time the INT pin will go low.
Hardware Connections:
Attach the Qwiic Shield to your Arduino/Photon/ESP32 or other
Plug the RTC into the shield (any port)
Open the serial monitor at 115200 baud
*/
#include <SparkFun_RV1805.h>
RV1805 rtc;
byte secondsAlarm = 0;
byte minuteAlarm = 0;
byte hourAlarm = 0;
byte dateAlarm = 0;
byte monthAlarm = 0;
void setup() {
Wire.begin();
Serial.begin(9600);
Serial.println("Alarm from RTC Example");
if (rtc.begin() == false) {
Serial.println("Something went wrong, check wiring");
}
rtc.setAlarm(secondsAlarm, minuteAlarm, hourAlarm, dateAlarm, monthAlarm); //Sets the alarm with the values initialized above
/********************************
Mode must be between 0 and 7 to tell when the alarm should be triggered.
Alarm is triggered when listed characteristics match
0: Disabled
1: seconds, minutes, hours, date and month match (once per year)
2: seconds, minutes, hours and date match (once per month)
3: seconds, minutes, hours and weekday match (once per week)
4: seconds, minutes and hours match (once per day)
5: seconds and minutes match (once per hour)
6: seconds match (once per minute)
7: once per second
********************************/
//rtc.setAlarmMode(7); //Once per second
rtc.setAlarmMode(6); //Once per minute
//rtc.setAlarmMode(5); //Once per hour: Alarm will go off every time there is a hundredths+seconds+minutes match (each hour)
//rtc.setAlarmMode(4); //Alarm goes off every day
rtc.enableInterrupt(INTERRUPT_AIE); //Enable the Alarm Interrupt
}
void loop() {
if (rtc.updateTime() == false) //Updates the time variables from RTC
{
Serial.print("RTC failed to update");
}
//String currentDate = rtc.stringDateUSA(); //Get the current date in mm/dd/yyyy format (we're weird)
String currentDate = rtc.stringDate(); //Get the current date in dd/mm/yyyy format
String currentTime = rtc.stringTime(); //Get the time
Serial.print(currentDate);
Serial.print(" ");
Serial.println(currentTime);
byte rtcStatus = rtc.status(); //Get the latest status from RTC. Reading the status clears the flags
if(rtcStatus != 0)
{
Serial.println("An interrupt as occured: ");
//Determine which bits are set
if(rtcStatus & (1<<STATUS_CB)) Serial.println("It's a new century!");
if(rtcStatus & (1<<STATUS_BAT)) Serial.println("System is on backup battery");
if(rtcStatus & (1<<STATUS_WDF)) Serial.println("Watchdog timer trigger");
if(rtcStatus & (1<<STATUS_BLF)) Serial.println("Battery is below threshold");
if(rtcStatus & (1<<STATUS_TF)) Serial.println("Countdown timer at zero");
if(rtcStatus & (1<<STATUS_AF)) Serial.println("Alarm went off!");
if(rtcStatus & (1<<STATUS_EVF)) Serial.println("External event detected");
}
delay(1000);
}
The last bit of code should tell me if the alarm has triggered without having to read the interrupt pin (but even when I do digitalRead the pin, nothing).
Everything else works…
Serial monitor:
15/02/2022 06:04:58PM
15/02/2022 06:04:59PM
15/02/2022 06:05:00PM
15/02/2022 06:05:01PM
15/02/2022 06:05:02PM
15/02/2022 06:05:03PM
Here was someone with the same problem: viewtopic.php?p=231486#p231486
When I paste his bit of code into the sketch the alarm works:
Serial.print(" InterruptMASK: ");
byte rtcStatus = rtc.status(); //Get the latest status from RTC. Reading the status clears the flags
const byte MASK = 0x12;
byte rtcIntMask = rtc.readRegister(MASK);
Serial.println(rtcIntMask, BIN);
Can someone please explain this to me 
Ok, so just in case someone has the same problems I had…
-
The alarm example is dodgy. Reading the status directly to check the interrupt seems to interfere with the setting of the bit by the RTC. Rather use the interrupt pin.
-
When using the countdown timer keep in mind that the input value is a byte. So setting the timer to countdown from eg. 500s won’t work correctly.
-
When using the countdown timer set to units of minutes, less than 3min doesn’t seem to work, rather use seconds.