Hi, I think that ESP8266 is damaged!!
I bought this component https://www.sparkfun.com/products/13678.
First test, i connected the ESP8266 with Arduino UNO and if i use 5V works fine,
ARDUINO UNO ESP8266
GND------------------GND
5V---------------------Vcc
No connected------ Reset
5V---------------------EN
2---------------------Tx
3---------------------Rx
Second test,if i use 3,3V the Rx pin works fine because the voltaje the Rx pin received of Arduino UNO is 4.78V.
ARDUINO UNO-------- ESP8266 ----------Volt
GND--------------------GND
3.3V---------------------Vcc
No connected--------- Reset
3.3V---------------------EN
2-------------------------Tx -------------------3.3
3-------------------------Rx ------------------4.78
Third test, i connected the ESP8266 with Arduino Pro mini at 3,3V but the Rx pin doesnt work? Somebody knows what happening? I reset the module, i restored as well.
ARDUINO Pro mini------- ESP8266 ------ volts
GND------------------------GND
3.3V-------------------------Vcc
No connected------ ------Reset
3.3V-------------------------EN
2----------------------------Tx --------------3.3
3----------------------------Rx --------------3.3
Somebody knows what happening? I need to update the firmware and how i can do?
I will appreciate your attention,
Many thanks.