Hi All,
Not sure if this is the correct place to post this, so would like to apologize in advance if it is not.
I recently puchased an Olimex SAM7-EX256 devel board. I went thru and installed the tools etc. I was basing my work off of Jim Lynch’s tutorial (which builds some code to flash 2-3 status LEDs). Based on output from the OpenOCD tool, it appears as though my flash programmer worked ( I even made sure I set the gpnvm bits ). However, when I reset the board, nothing happens. I was under the assumption that the HW was the same as when the tutorial was written. Now I am not so sure. Is there anyone here that could confirm/deny this. From the tutorial pages, I can see that the board design was definitely different. Jim also mentions 4 switches when it appears that the new board has two. When I went back and read the current SAM7-EX256 description, it appears that the only LED on the board is the power led ( which does come on :)). Also, upon cursory examination of the current SAM7-EX256 schematic, I do not see any mention of status LEDs.
In a nutshell, I need a way to do a quick board checkout to make sure that code (that I think has) downloaded to the board is actually running (and also to verify the HW components LCD etc). On the CD I rx’d with the ARM USB JTAG, there are a bunch of different projects – I specifically saw one for the SAM7256 board. Can anyone tell me if any of these projects will provide some kind of feedback that code is actually running on the board ( even a simple “Hello World” would be fine !!). Also, if the current design is different from previous designs, could someone post a link to the schematic of the older design
Regards
Victor