Finally I consider myself a lucky Olimex sam9-l9260 owner ![]()
There are however some… issues… I cant deal with on my own… yet ![]()
It seams I am still a beginner in terms of embedded linux ![]()
First problem i’ve encountered is related to the default debian installed on the board.
sam9-l9260:/# apt-get update
Get:1 http://ftp.uk.debian.org etch Release.gpg [386B]
Get:2 http://security.debian.org etch/updates Release.gpg [189B]
Hit http://ftp.uk.debian.org etch Release
Hit http://security.debian.org etch/updates Release
Err http://ftp.uk.debian.org etch Release
Get:3 http://ftp.uk.debian.org etch Release [58.2kB]
Err http://security.debian.org etch/updates Release
Get:4 http://security.debian.org etch/updates Release [37.6kB]
Ign http://ftp.uk.debian.org etch Release
Ign http://security.debian.org etch/updates Release
Get:5 http://security.debian.org etch/updates/main Packages [275kB]
Err http://security.debian.org etch/updates/main Packages
Sub-process bzip2 returned an error code (100)
Get:6 http://security.debian.org etch/updates/main Sources [47.8kB]
Err http://security.debian.org etch/updates/main Sources
Sub-process bzip2 returned an error code (100)
Get:7 http://ftp.uk.debian.org etch/main Packages [4155kB]
Err http://ftp.uk.debian.org etch/main Packages
Sub-process bzip2 returned an error code (100)
Get:8 http://ftp.uk.debian.org etch/main Sources [1217kB]
Err http://ftp.uk.debian.org etch/main Sources
Sub-process bzip2 returned an error code (100)
Fetched 96.4kB in 5s (16.5kB/s)
Failed to fetch http://ftp.uk.debian.org/debian/dists/etch/main/binary-arm/Packages.bz2 Sub-process bzip2 returned an error code (100)
Failed to fetch http://ftp.uk.debian.org/debian/dists/etch/main/source/Sources.bz2 Sub-process bzip2 returned an error code (100)
Failed to fetch http://security.debian.org/dists/etch/updates/main/binary-arm/Packages.bz2 Sub-process bzip2 returned an error code (100)
Failed to fetch http://security.debian.org/dists/etch/updates/main/source/Sources.bz2 Sub-process bzip2 returned an error code (100)
Reading package lists... Error!
E: Couldn't make mmap of 12582912 bytes - mmap (22 Invalid argument)
W: Unable to munmap
E: The package lists or status file could not be parsed or opened.
I have no idea how to deal with it ![]()
i red the but info at https://bugs.launchpad.net/debian/+sour … +bug/24626
but editing /etc/apt/apt.conf.d/30cache doesn’t help at all ![]()
Second problem is with my 2 GB SD card … I am trying to install gentoo on it…
i fount stage3 package for arm, unpacked it on the card. when I tried to emerge some stuff, it came shouting that there is no space left on the device 0_0
sam9-l9260:/karta# fdisk -l
Disk /dev/mmcblk0: 1981 MB, 1981808640 bytes
64 heads, 63 sectors/track, 960 cylinders
Units = cylinders of 4032 * 512 = 2064384 bytes
Device Boot Start End Blocks Id System
/dev/mmcblk0p1 * 1 823 1659136+ 83 Linux
/dev/mmcblk0p2 824 960 276192 82 Linux swap / Solaris
sam9-l9260:/karta# ls
bin dev home lost+found opt root stage3-arm-2008.0.tar.bz2 tmp var
boot etc lib mnt proc sbin sys usr
sam9-l9260:/karta# df -h
Filesystem Size Used Avail Use% Mounted on
/dev/mtdblock1 508M 104M 405M 21% /
tmpfs 30M 0 30M 0% /lib/init/rw
udev 10M 20K 10M 1% /dev
tmpfs 30M 0 30M 0% /dev/shm
/dev/mmcblk0p1 1.6G 905M 610M 60% /karta
sam9-l9260:/karta# touch dupa.txt
touch: cannot touch `dupa.txt': No space left on device
Any help will be appreciated ![]()
Merry Christmas and Happy New Year Everyone !!! ![]()