Hi,
I used the SAMD21 ProRF for the first time when I programmed it with a sketch and didn’t realize the serial monitor was connected. After the sketch was uploaded the Windows and Ubuntu systems were unable to recognize the USB device and this affects Arduino. The only way to upload a sketch is to put the chip into bootloader mode. In bootloader mode, the PC is able to recognize the device with no issue, I am also able to putty to the COM port. Is it possible to fix this issue, if so how? Also, how can I tell if the sketch is running ? I don’t see any of the TX or RX lights illuminate , I have closed the LoraWAN jumpers.
Mike