SAMD21 Pro RF unresponsive after upload

I am having the same issue.

The reset button does not appear to do anything at all.

I double-checked that the USB cables works - an Arduino feather using the same cable works fine.

The SAMD21 appears to be unresponsive - help!

julianrace,

Was this before or after uploading a program?

After. I tried uploading a basic example from your site (Lora Client code)

https://learn.sparkfun.com/tutorials/sp … 1589216464

After upload, the board is now unresponsive.

If it helps, using Mac OS 10.15.4 with Arduino IDE 1.8.13

Do you happen to remember the settings before programming?

It was fresh out of the box

My apologies, I was referencing the Arduino settings.

In the IDE I have the board set to “Sparkfun SAMD21 Pro RF”

The port was set to the usb serial port that came up when I first plugged in the ProRF (which is now not showing up)

Can you try closing out of the IDE and unplugging the Pro RF. Plug the Pro RF back in and hit the reset button twice to kick it into bootloader mode. Open the IDE back up and see if the board has a valid port.

I’ve tried that several times now. The board doesn’t seem to want to go into bootloader mode. I’ve tried super quick double press of the reset button, slow double press, very slow double press and and still nothing - the board doesn’t respond. Here’s the USB devices my Mac sees:

MacBook-Pro:~ sto$ ioreg -p IOUSB -w0

±o Root <class IORegistryEntry, id 0x100000100, retain 23>

±o AppleUSBXHCI Root Hub Simulation@00000000 <class AppleUSBRootHubDevice, id 0x1000003ee, registered, matched, active, busy 0 (6 ms), retain 12>

| ±o USB3.1 Hub@00100000 <class AppleUSBDevice, id 0x10001098f, registered, matched, active, busy 0 (0 ms), retain 12>

±o AppleUSBXHCI Root Hub Simulation@01000000 <class AppleUSBRootHubDevice, id 0x1000003f5, registered, matched, active, busy 0 (6 ms), retain 8>

±o AppleUSBXHCI Root Hub Simulation@14000000 <class AppleUSBRootHubDevice, id 0x100000436, registered, matched, active, busy 0 (6 ms), retain 9>

| ±o USB2.1 Hub@14100000 <class AppleUSBDevice, id 0x1000109aa, registered, matched, active, busy 0 (0 ms), retain 14>

| ±o BillBoard Device@14120000 <class AppleUSBDevice, id 0x1000109c7, registered, matched, active, busy 0 (2 ms), retain 13>

| ±o USB Receiver@14130000 <class AppleUSBDevice, id 0x1000109db, registered, matched, active, busy 0 (7 ms), retain 16>

±o AppleUSBVHCIBCE Root Hub Simulation@80000000 <class AppleUSBRootHubDevice, id 0x10000044c, registered, matched, active, busy 0 (8 ms), retain 15>

±o Apple T2 Controller@80100000 <class AppleUSBDevice, id 0x10000044e, registered, matched, active, busy 0 (9 ms), retain 14>

±o Touch Bar Display@80600000 <class AppleUSBDevice, id 0x100000462, registered, matched, active, busy 0 (7 ms), retain 13>

±o Ambient Light Sensor@80300000 <class AppleUSBDevice, id 0x100000468, registered, matched, active, busy 0 (10 ms), retain 11>

±o Headset@80400000 <class AppleUSBDevice, id 0x100000470, registered, matched, active, busy 0 (8 ms), retain 11>

±o Touch Bar Backlight@80700000 <class AppleUSBDevice, id 0x100000478, registered, matched, active, busy 0 (9 ms), retain 11>

±o FaceTime HD Camera (Built-in)@80200000 <class AppleUSBDevice, id 0x100000480, registered, matched, active, busy 0 (10 ms), retain 15>

±o Apple Internal Keyboard / Trackpad@80500000 <class AppleUSBDevice, id 0x100010905, registered, matched, active, busy 0 (15 ms), retain 20>

And again but with the feather plugged in

MacBook-Pro:~ sto$ ioreg -p IOUSB -w0

±o Root <class IORegistryEntry, id 0x100000100, retain 23>

±o AppleUSBXHCI Root Hub Simulation@00000000 <class AppleUSBRootHubDevice, id 0x1000003ee, registered, matched, active, busy 0 (6 ms), retain 12>

| ±o USB3.1 Hub@00100000 <class AppleUSBDevice, id 0x10001098f, registered, matched, active, busy 0 (0 ms), retain 12>

±o AppleUSBXHCI Root Hub Simulation@01000000 <class AppleUSBRootHubDevice, id 0x1000003f5, registered, matched, active, busy 0 (6 ms), retain 8>

±o AppleUSBXHCI Root Hub Simulation@14000000 <class AppleUSBRootHubDevice, id 0x100000436, registered, matched, active, busy 0 (6 ms), retain 9>

| ±o USB2.1 Hub@14100000 <class AppleUSBDevice, id 0x1000109aa, registered, matched, active, busy 0 (0 ms), retain 15>

| ±o BillBoard Device@14120000 <class AppleUSBDevice, id 0x1000109c7, registered, matched, active, busy 0 (2 ms), retain 13>

| ±o USB Receiver@14130000 <class AppleUSBDevice, id 0x1000109db, registered, matched, active, busy 0 (7 ms), retain 16>

| ±o Feather 32u4@14140000 <class AppleUSBDevice, id 0x10002907f, registered, matched, active, busy 0 (6 ms), retain 15>

±o AppleUSBVHCIBCE Root Hub Simulation@80000000 <class AppleUSBRootHubDevice, id 0x10000044c, registered, matched, active, busy 0 (8 ms), retain 15>

±o Apple T2 Controller@80100000 <class AppleUSBDevice, id 0x10000044e, registered, matched, active, busy 0 (9 ms), retain 14>

±o Touch Bar Display@80600000 <class AppleUSBDevice, id 0x100000462, registered, matched, active, busy 0 (7 ms), retain 13>

±o Ambient Light Sensor@80300000 <class AppleUSBDevice, id 0x100000468, registered, matched, active, busy 0 (10 ms), retain 11>

±o Headset@80400000 <class AppleUSBDevice, id 0x100000470, registered, matched, active, busy 0 (8 ms), retain 11>

±o Touch Bar Backlight@80700000 <class AppleUSBDevice, id 0x100000478, registered, matched, active, busy 0 (9 ms), retain 11>

±o FaceTime HD Camera (Built-in)@80200000 <class AppleUSBDevice, id 0x100000480, registered, matched, active, busy 0 (10 ms), retain 15>

±o Apple Internal Keyboard / Trackpad@80500000 <class AppleUSBDevice, id 0x100010905, registered, matched, active, busy 0 (15 ms), retain 20>

MacBook-Pro:~ sto$

SAMD21 PRO RF UNRESPONSIVE AFTER UPLOAD of ttn-apb

After double click I can see the serial port, after programming there no serial port, the USB shows the port failed

Windows has stopped this device because it has reported problems. (Code 43)

ttn_abp_node_hello_world instead of the lorawan ttn_abp fixed this problem, the trick was SerialUSB instead of Serial

@sobellinni – Your insightful post ponied me to the right direction, Spark Fun is sharing a defective example with the board manager published to the IDE. I got the example you mentioned from GitHub and all is well! Thank you

@SparkFun staff - kindly address this repetitive issue with the examples! It would save others the same hassle!