The [MicroMod SAMD51 schematic shows nets SCK1, COPI1, CIPO1, and CS1 are wired to the MCU, but they are not wired to the M.2 pins. I would expect them to be wired to M.2 pins 60, 62, 64, and 70, respectively, but this is not shown on the schematic. Is this a bug in the schematic, or are the pins actually not connected?
I have one of these on order, so I should be able to confirm this myself once it arrives.](https://cdn.sparkfun.com/assets/6/2/4/0/0/MicroMod_SAMD51_Schematic_v1_3.pdf)