Hello, I am attempting to design a PCB that will have an M.2 connector accepting the ZED-F9P module and connect to a Raspberry Pi Zero 2 W. I am aware of the schematic for the main board that shows the connector nets with the function board but I cannot find anything that shows what actual pins in the M.2 array they correspond with. Is there a diagram that relates the MicroMod connector with the nets each pin belongs to? Any help is appreciated.
Scroll down to the colorful section here MicroMod GNSS Function Board - ZED-F9P Hookup Guide - SparkFun Learn where there is a table listing them ![]()
You can also use Autodesk Eagle to open the board files and see the actual routes and whatnot if needed