I’ve been comparing this sensor to some DHT22 sensors that I have. All my DHT22s report the same values within the precision of the data sheet. I have no way to independently verify their accuracy. The SCD30 reads 1.5-2 degrees higher, so this difference is outside the accuracy range of their datasheets. I can adjust the SCD30 temperature reading using the temperature offset. But even after that, the SCD humidity reading is about 10-15% lower in relative terms, 10% in absolute terms, to the DHT22.
Has anyone tested the accuracy of either the DHT22 or SCD30 for temperature or humidity or compared them to a know accurate source.
TIA,
Evan.