SD card sniffer - not locking into slot due to design oversight?

I’m using this SD sniffer https://www.sparkfun.com/products/11468 to, well, sniff SD card traffic. The issue is that many devices’ SD card slot use the same push-push slot that’s on this sniffer, and that means in order to lock the card in place, there needs to be a cutout to activate the spring mechanism in the card slot.

Standard SD cards have 2 cutouts on both sides, with one side being the write protect toggle. I believe that’s what the card slot is utilizing to lock the card. The sniffer doesn’t have that, so whatever device I plug that into, will not be able to lock the card in place if it’s using the same push-push slot. Unable to lock = unable to sniff.

Is this a design oversight or what? I get that you(sparkfun or whoever designed this, as it seems sparkfun didn’t design this themselves) may need to account for write-protect presented to host device, but it’d be nice if something is done to accommodate the push-push type of SD card slot.

Sounds like it’s a bad SD card slot. You may proceed for replacement if the warranty is still valid.

I bought the sniffer to check what my camera was requesting from the card on boot, and as soon as I plugged it in, it damaged the camera’s slot. The lack of the standard notch (which I didn’t notice ahead of time) seems to have broken the locking mechanism on the slot, and potentially more.

Very disappointed, it’s probably going to be a very expensive repair, if it’s possible to get the right parts to repair it at all.

Hopefully the next person finds this post first. It should really be mentioned in the product description.