I have an Artemis Openlog which I’ve interfaced to a NEO-M9N GPS board via QWIIC. I can read the info from the NEO-M9N and display it on my PC screen in a serial monitor after fudging the I2C pinouts. I’m now trying to write that data to the SD card on the Openlog board.
First I tried some of the SD examples but I didn’t get them to work as the SPI pinouts are different on the Openlog board and I was getting errors about MISO and MOSI etc not being defined. I didn’t think I would have to modify library files to assign pinouts - I thought the thing about Arduino was that the legwork has been done and now you just write code and marvel at your success…
If gave lots of compile errors and won’t even complie. I’ve also tried some of the examples here:
OpenLog_Artemis/Firmware/OpenLog_Artemis/
But still get lots of compile errors.
I’ve written plenty of code before but I’m new to Arduino and especially new to SD writing so I’m at a loss how to make it work. The libraries seem to be a jungle. Has anyone had any success writing to an SD card with the Artemis Openlog? What I want to do is quite simple: press a button on the Openlog board and log the data coming off the GPS board then stop logging on a second press of the button. I can do the rest but the SD stuff has me beat.
Would I be better off getting the older, simpler Qwiic Openlog?
Select SparkFun RedBoard Artemis ATP from the boards list
The example shows how to power up the SD card from microSDPowerOn() helper function
You’ll need to install Bill Greiman’s SD library: https://github.com/greiman/SdFat-beta to get the example to compile. (Arduino’s built-in SD library is pretty terrible)
Any SD card formatted to FAT16 should work. Keep it under 32GB. OLA supports larger cards but let’s no go there for now.
Thanks for that. I downloaded the SDFat_Beta library and deleted the SDFat library I had installed before (ie the non Beta). When I went to the library manager it showed the original SDFat library versions but not the SDFat_Beta version 2.0. Is that odd? I have checked and the original SDFat library files etc are all gone, so I don’t understand why it’s not reading the library.properties file and showing version 2 Beta.
OK, had to make a few small changes to get it to compile but it does now. I also managed to compile & run some of the examples.
Are there any simpler examples of how to just create a file on the SD card and write to it? All of the examples in the SD-FAT_Beta library seem a bit over the top for what I want to do - or perhaps I’m hoping it’s a lot simpler than it really is?