I have a LPC-P1 and the ARM-JTAG. I use crossstudio as IDE. I set the PINSEL for JTAG. But the Wiggler says, that the target is not responding. Did you try this? Is there a problem with the TDO/P0.31 pin? what should i do with the rtck-pin of the ARM-JTAG? I open DEBUG-JTAG and BSL- jumper.
Because LPC-P1 uses primary JTAG interface, just forget PINSEL. RTCK is driven by debugging software. P0.31 is button input, you can use it in your application.
There are some settings:
DEBUGGING and CHIP PROGRAMMING via JTAG:
Settings for CrossStudio:
Targets = Macraigor Wiggler (20 pin)
Jumpers on LPC-P1:
DBGSEL short, BSL open
CHIP PROGRAMMING with Philips Flash Utility via RS232:
Jumpers on LPC-P1:
DBGSEL open, BSL short, push RESET (smaller button) when asked