Selecting a wireless module

I’m planning to integrate some wireless communications between two of my robots. However, I have no experience or knowledge in wireless stuff. Basically, I just want to send some data from one ATMega32 to another ATMega32, which are always at the most 3 metres apart.

I don’t know which modules are suitable for my use. How do I communicate with the modules? Also, If I get two transmitters and two recievers with the same frequency, will I have to get some sort of channel thingy going on to distinguish between the two transmitters and recievers? Would it be better to get a transciever?

for simplicity

consider

http://maxstream.net/products/ $20@1ea module. Transparent serial port extension via RF. Each radio has a MAC address. Or you can run ZigBee routing.

Similar, from

http://www.helicomm.com/?page=2-35&PHPS … e6ab745bbd

or the Jennic modules on this website.

also Bluesmirf or another bluetooth setup would be great, there’s some cool bluetooth serial modems in the SFE product listing which I highly recommend.