Sending analogue signals via WI FLY GSX module

Hi,

I am new to sending sensor data via WI-FI and I am trying to get a bit more information on the WI FLY GSX module. The aim is to send data from strain gauges and an accelerometer via WI-FI using the WI Fly GSX module. I was planning to use the analogue sensor inputs on the WI FLY module for the analogue voltage signals from the two Wheatstone bridge and 3 axis accelerometer, so 5 signals total. Is it as simple as just connecting to the sensor inputs directly from the output of the strain gauges and accelerometer or do I require any further modules or programming for the WI-FI?

Cheers