setup RTK System with 2 GPS-RTK

Hi Guys

Was anyone able to setup the GPS-RTK boards to get precise location?

We are struggling arround since 2 days. The plan is to use 2 GPS-RTK boards and use one as base station and one as “rover”

doesn’t matter if it takes 1 or two arduinos, raspberry pis whatever. we would just be happy to see that RTK LED blinking on these devices…

Thank you in advance

Hi swissrope,

You should be able to set two of the RTK boards up with one as a base and one as a rover. [This example will set up one module as a base station and [this section of our Hookup Guide goes over some more details on how to push the RTCM data to your rover. Have you tried piping RTCM data directly to one of the GPS-RTK’s from a correction source? u-center has a nifty tool for setting that up easily or you can follow the instructions we have in [this section of the Hookup Guide. The [u-center User’s Guide is another good resource that will help you get RTCM data through u-center.

If you are having trouble following that guide or the other documents I linked above, can you please provide some more information on how you are using the GPS-RTK board as well as what troubleshooting steps you have already tried? Information about what type of Arduinos you are using, what examples you are using from the u-blox library will also be helpful for us to troubleshoot.](https://www.u-blox.com/sites/default/files/u-center_Userguide_(UBX-13005250).pdf)](https://learn.sparkfun.com/tutorials/gps-rtk-hookup-guide#connecting-the-gps-rtk-to-a-correction-source)](https://learn.sparkfun.com/tutorials/gps-rtk-hookup-guide#setting-up-a-base-station)](SparkFun_Ublox_Arduino_Library/examples/NEO-M8P-2/Example2_StartRTCMBase/Example2_StartRTCMBase.ino at master · sparkfun/SparkFun_Ublox_Arduino_Library · GitHub)