I have the SparkFun M6E Nano Simultaneous RFID Reader. I’m trying to use JADAK’s Universal Reader Assistant along with a CH340 USB-Serial adapter. I can get the board to ‘connect’ and, when I hit the ‘Read’ button, it disconnects from UBS and I get the following message 'Access to the port ‘COM6’ is denied. BTW, COM6 is the correct USB port.
Also, I’ve confirmed my CH340 USB-Serial adapter is working (on another device/application).
More info: If I set the reader to ‘Read Continuously’ and set the RF OFF time to something > 0, the comm failure seems to happen at the exact time as RF OFF time. Example: RF OFF = 10,000, the failure happens pretty close to 10 seconds after I hit the read.
Any suggestions?