I recently bought the Simultaneous RFID Tag reader (M6E Nano) for use in a school project, and attached it to the CH340C breakout, and am using a USB-C Cable to connect to my USB port in the computer, as instructed by following the tutorial available in the RFID reader. https://learn.sparkfun.com/tutorials/si … troduction, following the “Using Universal Reader Assistant” system.
I have verified the soldering work on the, continuity doesn’t appear on any of the 6 header ports, attached work here:
When starting up the Universal Reader Assistant (URA), the program is able to recognize the connection of the device, and changes COM ports when connected to the different USB ports. Have also tried different USB-C to USB cables, all are able to find the Reader once the Refresh button is pressed.
After setting the power levels to 3-5 dBM (due to only using USB power currently). I connect the system and notice that doing Read Continuously or Read N Tags, I end up with the system forcibly closing on me, with the LED also turning off:

When Doing “read once”, I can read a RFID tag at close range:
Note that after pressing the Read Once button 4 times, the COM port disconnected and said that access to port is then denied: Most likely too much traffic?
I have reached out to Jadak support for anything on the URA, and they said that on the Transports Logs I sent (attached here), there is nothing that they can see wrong with the software side of the connection.
I also checked the USB Device Analyzer, and didn’t see anything that could indicate a switch in USB connection (no logs sent). The information for those ports can be attached if necessary.
Anything else I should be looking into, or more likely that the board is dead? I will be testing on another device soon, but for now, I wanted to see if there was anything else I can with my current setup.
Thank you, Ryan Tanary