I have installed a hydronic radiant heating system that’s embedded in concrete Alabama this includes a snow melt system on concrete stairs.
I have thermocouples already in place. These include incoming and outgoing temps at the heat exchanger and slab temps in different zones.
I want to set up a dedicated tablet that displays graphical data on the temp so I can see the heat times and latent heat capacity of the slabs. so I would need datalogging of 6 or 8 sensors.
So I was looking at the sparkfun blynk board and to use the blunk app to easily do the graphics. But I have no clue how to set this up from the hardware side. A bit out of my league with these kinds of boards. Of course there’s no example of multiple analogue inputs since this is a pretty specific task.
Can you please recommend which boards I would need and how to set it up the multiple temp sensors so I can run Blynk to graph them.
Thanks,
Jamie