Smaller Hantouch Panels for the Colo(u)r Nokia LCD

I was pleasantly surprised when you started selling resistive touchscreens for the PSP LCD. I just thought it would be nice to complement that with Hantouch’s smallest touch screen - the HT019A-NCIAB72. It will fit well with the Nokia LCD (1.9") and could be really useful for an upcoming project.

Keep up the great work

I’d love to see that touchscreen too, as well as their 2.2in one. I desperately need something that size for a project, but no one seems to carry anything close

A small touchscreen for the 128x128 1"x1" OLED display would be nice too.

I agree the touchscreen for the OLED is a good idea.