smd header pin?

McXavier:

smdFan:

leon_heller:
Don’t you mean 2.54 mm (0.1")?

Leon

On the development board of ATmega128, I measured the pins that are connected to AVR ISP programmer cable with a caliper. It turned out to be 2.50 mm. What I want is header pins that can be connected to the cable of ISP programmer for programming. Thanks

Did you measure them inside-to-inside? Measuring male header pitch is a two-step process with calipers, (inside_to_inside + pin width) or (outside_to_outisde - pin width).

If you look inside the .pdf file: http://www.sparkfun.com/datasheets/AVR/avr-h128b.pdf you will see, it states the pins have a 0,1" pitch.

check out page 167 of the digikey catalog: http://dkc3.digikey.com/PDF/T081/0167.pdf

Thanks everybody. Your answers were very helpful. I think my measurement of 2.50 mm is wrong and I will go with the 2.54 mm. Thanks a lot.