Dear all,
I am currently testing my smol Artic R2 board - currently without an active CLS account.
As a test I have uploaded the Example 3 that comes with the board. In the serial monitor I get the following messages:
firmware status IDLE flag is set. The firmware is idle and ready to accept commands.
TX configuration: ARGOS PTT-A3.
RX configuration: ARGOS 3.
The Satellite Detection Timeout is 600 seconds.
Starting satellite detection…
ARTIC R2 Firmware Status:
The firmware status BUSY flag is set. The firmware is busy changing state.
ARTIC R2 MCU instruction result:
MCU command result: success. The configuration command has been accepted.
ARTIC R2 Firmware Status:
The firmware status BUSY flag is set. The firmware is busy changing state.
The firmware status INTERNAL_ERROR flag is set. An internal error has occurred.
The firmware status DSP2MCU_INT2 flag is set. Interrupt pin 2 is high.
INT2 pin is high. Satellite detection has timed out!
ARTIC R2 instruction progress:
MCU Instruction Progress: INTERNAL ERROR!
Satellite detection is complete! Freezing…
What do these lines mean?:
The firmware status INTERNAL_ERROR flag is set. An internal error has occurred.
ARTIC R2 instruction progress:
MCU Instruction Progress: INTERNAL ERROR!
Is my board defective? Or is there something I have to modify? I have already considered whether I should install a new firmware. But the board is brand new and if it might run unstable right now, I didn’t want to break more without asking.
I would be very thankful for your advice.
Best regards
Ceal