Solar iPhone charger

Hi,

I’m trying to build a small system for charging my cell phone with a solar panel. This includes:

  1. Solar cell (5 W in full sunlight, it’s a CIGS cell)

  2. A Sparkfun Solar Buddy charger

  3. 2000 mAhr 3.7V Li-ion battery

  4. TK0445 DC-DC 3V to 5V buck/boost converter with a USB female jack

Before trying to charge with the solar cell, I fully charged the Li-ion battery and plugged it into the Solar Buddy. On the LOAD terminals, I measure a voltage of 3.79 V, so I know that’s working. I connect two leads to the LOAD terminals to my DC-DC converter, which converts the voltage to 5.2 V. With a multimeter, I read 5.2 V across the USB terminals that correspond to +5V and ground. Then I plug in my iPhone 5 USB cable, and at the end of those leads I also read 5.2 V.

One would think that plugging my iPhone in, it would start charging. However, it’s not charging. Is the 5.2V too high? Am I missing another component in this circuit?

Thank you for your help!

Some, if not all, Apple products require certain voltages to be present on the USB data lines in order to charge. Google will point you toward the details, but Adafruit has a tutorial somewhere.