ctrc
April 29, 2013, 12:18pm
1
I have the Pro Micro - 5V/16MHz with ATMega32U4.
I am trying to upload a Sketch.
I always get “avrdude: stk500_getsync(): not in sync: resp=0x00”
http://uppix.net/3/7/6/a5ce405cd868c5e5 … f7cb6a.jpg
What Tools>Board should I choose ?
“Arduino Pro or Pro mini (5V, 16 MHz) w/ ATmega328” doesn’t not seem to be the correct one…
ctrc
April 29, 2013, 12:40pm
2
I choose LyliPad Adruino USB as board.
I successfully uploaded the “Blink” sketch.
Win 7 detected the board as a new device (drivers were already installed).
Now it is just showing a “unknown Device” and I am not able to re-instal the SparkFun ProMicro.inf drivers.
It keep saying that the driver are not compatible…
http://uppix.net/b/0/2/49de56aea5d28301 … bd9ba9.jpg
Looks like it was not a good idea to choose LyliPad as the board…
Rebooting or using libusb-win32-bin-1.2.6.0 doesn’t help.
http://uppix.net/6/c/5/8aeb898db6e1550c … e70c4f.jpg
uChip
May 1, 2013, 5:19pm
3
There is an add-on to Arduino for the Pro Micro. The link to the add-on is on the Sparkfun product page. Once you install the add-on you can select “SparkFun Pro Micro 5v/16MHz” from the board menu. Instructions are on the “Getting Started Tutorial” also linked from the product page.
Good luck!
ctrc
May 5, 2013, 5:45am
4
So I bought a new Pro Micro and did a fresh windows install.
I plugged the new board, installed the driver, selected “Pro Micro 5v/16Mhz”, uploaded a sketch, I got an error…
avrdude: ser_send(): write error: sorry no info avail
I tried plugin in my previous board, it appeared as "vmware device' ? ?, I installed the driver, but I got the same error as previously mentioned.
I plugged the new board again. It showed up like this : http://uppix.net/3/d/c/356d8b921c687b0b … 57b506.jpg
I installed the same driver again and I got a big fat old blue screen…
http://uppix.net/6/9/f/3ec82956320626fd … 90f1c2.jpg
ctrc
May 5, 2013, 5:52am
5
Problem fixed.
I unplugged it and plugged it again. Waited a few second and the board appears on COM5 without any problem.
Upload of sketch was successful
Thank u for your help uChip !
Has posting a picture of the BSOD helped anyody…EVER?