I installed python packages for pHat on my rasp 3 and mounted hat to it.
using USBC to power, blue light on board blinks, go servo examples to work, actually got motor examples to run but the motors do not work. I used the encoder motors first and then switched to simple DC motors-same result.
The Sparkfun Qwicc packages and sparkfun-qwiic-scmd seem to work ok with python, it is like the motors aren’t activated.
IMG_6338.jpg -this is the original setup .It has dual blue motors with encoders and a servo. Servo works, motors do not.
I have pictures of scope which show 0-scope PWM during dual motor python demo and then my regular yellow DC motor hook up without encoders --but I keep getting HTTP errors when uploading. Bottom line these regular motors work!
I took the blue motors and hooked directly to power supply just motor + and- , again they do not work.
The motors I purchased from Sparkfun are not functional.
I think we had a recent issue from the manufacturer with the cable colors not being consistent for the motors with encoders. If you are following the Auto pHAT hookup guide, I added a picture with the pin connections for the motors with encoders to assist with that. Hopefully, that helps get those working.