SparkFun Bluetooth Modem - BlueSMiRF Silver multiple connections

Hi,

I have been trying to establish multiple bluetooth connections with several SparkFun Bluetooth Modem - BlueSMiRF Silver modules.

I need four module slaves to be connected to one module master.

The command reference says this:

"Only one client can connect to a slave module at a time. As a master, the

module can make multiple connections, but only in a point-to-point, serialized fashion. Roving Networks modules do not currently support multi-point

master mode."

I don’t quite get how can i make multiple connections with one module, and if it is possible.

Thanks.

You can only make one connection at a time. You could connect to one device, disconnect and then connect to another but you can’t connect to multiple devices simultaneously.