Running the Bluesmirf in multi-point mode maximum 2 connections (broadcast).
Data flows into UART from 3rd party serial device and streams out to connected “masters/clients” so Bluesmirf is acting as Slave/Server.
However, if either of the connected clients disconnect, both connections are closed and the other client is disconnected without cause.
Is there a setting somewhere I have missed? the Bluesmirf only accepts 2 connections (COM0 and COM1), 19200 with 8 data, No parity, 1 stop and no hardware handshake (RTS/CTS soldered together).
It also has ATSW24,2,0,0,0 (No Response Except For Events) and ATSW25,0,1,1,0 (data mode, Ignore Data While Unconnected) settings.
I hope to hear from someone who can explain this. The adapter would fill our requirement perfectly if the connections wouldn’t be terminated like this.
Thanks in advance…Yves