I recently ordered this product from you and the Red board and the Arduino shield for it.
I have wired it up as described. I have installed the libraries for Spark Fun Laser distance sensor and I have managed to upload the first demo: Example1_ReadDistance and it gets as far as:
Serial.println("VL53L1X Qwiic Test");
and prints this to the serial monitor but it doesn’t seem to do anything beyond that.
It appears that is fails when it gets to ```
distanceSensor.begin()
I have tested that the board is working fine with the basic blink example.
I have noticed that the red power light on the sensor doesn't always come on and stay on. I'm not sure if this is normal. Sometimes it comes on if I fiddle with the siting of the shield on the board. Is this a loose connection issue?
I bought the Red board because I thought it would solve the problem of the connection between my Arduino Uno, the shield and the sensor.
I would really like to resolve this soon. Any suggestions or ways I can debug the problem?