SparkFun GPS Breakout - XA1110 (Qwiic)

I am trying to code a driver to read data from the GPS module but I want to use interrupt control instead of polling. I soldered a wire to the INT_N pin but I do not see this toggling. Can someone please confirm the INT_N functionality is supported with this device? Is there a command that needs to be sent to enable this function?

Any help is greatly appreciated.

Thanks!

Burke

The datasheet indicates that this pin should go HIGH when a full NMEA packet is saved in the buffer. Can you confirm if the packages are complete?