I’m very much a noob. I’ve had the assistance of seasoned programmers help create a data logger. I don’t want to keep bugging them though. They feel the logger may be faulty. No config file seems to ever be created. And when they created one, and intentionally input a wrong baud rate , the config file was never fixed when it rebooted. Any help?
purchased from the SparkFun website a month ago. Its hooked up to a nano. both stat lights with a 16gb sd card inserted are on and steady (not blinking).
No errors just doesn’t write to the sd card, Have tried multiple cards as well. Odd thing is the blue and the green led’s are lit, BUT they are stead and dont go on/off, flash, they are steady on. Also, there is no config file on the sd card??? thoughts?
Hey Paul, it’s not definitely not the board. I just received a replacement of the same board, and nothing is writing. I’m not even showing a config on the microsd which leads me to believe its a coding issue on my end.
It’s all on a breadboard right now, I have the open logger hooked to a nano with the following connections: