SparkFun Quadband GNSS RTK Breakout - LG290P (Qwiic) firmware upgrade error

I just receiver our SparkFun Quadband GNSS RTK Breakout - LG290P (Qwiic) boards.
Following “Firmware Upgrade Guide” I used QGNSS V2.0 to upgrade the firmware of the two boards Quectel_LG290P_Firmware_Release_V0104S.zip from … SparkFun_RTK_Postcard/Firmware at main · sparkfun/SparkFun_RTK_Postcard · GitHub

Unfortunately the update process did not succeeded… on the firmware download tool I get:
[17:11:34.355] Ready
[17:11:47.790] LG290P(03):UPG
[17:11:47.829] V1.0.3 Jul 2 2024 13:15:53
[17:11:47.830] Enter flash tool
[17:11:47.831] kt5030 entry function
[17:11:47.831] Port: COM9
[17:11:47.832] Baud rate:460800
[17:11:47.832] Module: LG290P03
[17:11:47.832] Firmware:C:/Users/joel.brenner/Downloads/LG290P03AANR01A04S.pkg
[17:11:47.832] Connect…
[17:11:47.832] Synchronize…
[17:12:07.859] Sync the serial failed,err: 0x400
[17:12:07.861] ql_flash_tool upgrade fail,ret:[-1]

The board is configured as base station and is emitting RTCM messages on COM9 (visible on QConsole)

Any idea about what could the problem be? Why the update fails ?
Thx, Joel

The output message is missing, try re-posting it

Which firmware is loaded now?

$PQTMVER,1,MODULE,LG290P03AANR01A03S,2024/05/22,18:09:06*36

There is no output message emitted by Firmware Download dialog … it simply passes from red square icon to the green arrow by showing the already posted messages on the console

Here:

and

&

Saluti

1 Like

@bamarcant,
Or simply momentarily ground the RESET pin on the module J10 connector to reset the LG290P within the 20 sec delay period.
Regards,
TCIII

2 Likes