I have a SparkFun RTK Express running System Firmware: v3.2-Mar 8 2023.
When I scroll through the options by clicking on “setup”, I am presented with the following:
mark
rover
base
bubble
config
e-pair
ap mode (profile)
wifi mode (profile)
Profile3 (profile)
Profile4 (profile)
My first question is what does “e-pair” mean and how is it used?
My second question is how can I delete the entries “Profile3” and “Profile4”? I created four profiles, but now I only need the first two (ap mode and wifi mode). I can reset profile 3 (Profile3) and profile 4 (Profile4), but I canont delete either profile name. When I try to delete the profile name, I am presented with the following error message: “Error: Must be 1 to 49 characters”
Thanks for any guidance on either of these questions.
That creates a separate file containing the coordinates of the mark that was just created. It’s basically a shortcut to avoiding using GIS software and just ‘go headless’.
When the Marks feature is enabled a file is created on the micro SD card with the file name “Marks_date.csv”, specifically “Marks_year_month_day.csv”. As an example: Marks_2023_10_19.csv. This file contains comma separated data with the first line being the header containing the column names. Each line of data includes:
- Year-Month-Day
- Hour:Minute:Second
- Latitude
- Longitude
- Altitude in meters
- Number of satellites in view
- Horizontal position accuracy in meters
- Battery level (percentage)
- Battery voltage
Each time the Mark entry is selected using the “Setup” or “Power” button, a line is written to this file.