hi, i want to connect the rfid module to the redboard via serial, which gpio should i use? how do i set the SoftwareSerial function softSerial(3, 1) ?
I am bit puzzled what you want to do?
There are a lot of posts about the M7E in this forum that contain information on how to connect. (like M7E Hecto Simultaneous RFID Reader Not Communicating - #4 by paulvha) Apart from that there is the hookup guide.
Setting SoftwareSerial as (3,1) does not make sense. The RX would become pin 3, and TX would become pin 1. BUT pin 1 is already used as TX for USB to connect to your PC.
I connected the rfid module to pins 2 and 3 of an arduino uno, I moved the resistor and in the code I used softserial(2,3), but it still doesn’t work, any other tips to pay attention to?
I am trying the range_test example and the output is as follows Module continuously reading. Asking it to stop…
Module failed to respond. Please check wiring.
Happens often, so let’s see :
- How did you connect ?
- Is the UART switch set to Ser?
- Is the M7E power led on ?
- Pictures ?
" I moved the resistor "which resistor is that ?