SparkFun TFT LCD Breakout - 1.8" (128x160) -alternate LCD

Would it be possible to use the SparkFun TFT LCD Breakout - 1.8" (128x160) PN:LCD-15143 breakout board with a wider LCD?

Hi Bwhite,

I’m afraid that’s not something SparkFun Tech Support has an answer for. The driver IC on the breakout only works for specific a specific display resolution and the breakout was designed to work with the display that comes with the board. If you wanted to do some research to see what other displays might work with this breakout, the best place to start would probably be the [ILI9163C LCD Driver Datasheet.](https://cdn.sparkfun.com/assets/4/e/b/7/6/ILI9163C.pdf)