Hi all,
Does anyone know what antenna in the OPUS antenna pull down menu is the same as the SPK6618H?
Hi all,
Does anyone know what antenna in the OPUS antenna pull down menu is the same as the SPK6618H?
The HFX6618 antenna looks like a suitable alternative. It utilizes an older version of the same 6618 base element.
great thanks, i dunno why sparkfun doesn’t want to provide such info upfront, maybe their stuff is just for more advanced users interested in spending hours looking for crucial information.
This info in on the forum and in the OPUS dropdown box.
If you ever get stuck, you can search the Calibrations database here:
In OPUS, it looks like this:
The OPUS list isn’t strictly alphabetical, so it’s a little fuzzy.
Also, this is a great time to point out the differences in the (2) antennas mentioned, according to the NGS Calibrations.
From the Calibration Files
Top106 [vs SPK8818]
Actual L1 Phase Center
2.66mm [vs 0.47mm] North
-3.23mm [vs -1.26mm] East
52.94mm [vs 48.02mm] Up
Actual L2 Phase Center
-0.29mm [vs 2.73mm ] North
3.54 [vs -1.87mm] East
48.05mm [vs 35.91mm] Up
Looking at the Calibration files, it’s also easy to see how “Not” using the North Arrow Reference Mark can quickly add half a cm error to a solution, before you even get started ![]()
This is the case for any antenna.
thanks for the info guys!
I’m stuck on sending opus my data.
I collected about 800 files with pygpsclient on my pi and i concatenated them into one file.
opus didn’t like it
I’m going to retry with only an hours worth of observations.
I wonder if picking a few log files from each hour out of the 24 recorded would be a good strategy?
OPUS has A LOT of built-in data validation and checks… and is therefor very particular about the input file.
This seems extremely optimistic to me. I’ve used OPUS many times, but I’m FAR from an expert.
If you are just starting out with OPUS [sorry for an assumption] , you may want to start with a 2 hour continuous mission recording the RAW GPS L1 & L2 Observables. Submit one RINEX file. There are a few great posts on this forum with tips & tricks using RtkConv to Generate the RINEX that OPUS will like.
Plenty of folks here can help ya… and good luck ! ![]()
Just record binary with pygpsclient?
Then rtkconv
@steve1428 - I’m not a PyGPSClient user, so I can’t offer any help with that ![]()
You might get better results if you start a specific thread.
That will also help other people in the future when they are searching the forum for a similar answer.