Standalone Arduino Attendance Monitoring System

Good day Folks,

I am planning to fabricate and develop a standalone arduino attendance monitoring system for our school. I will just ask if it is possible. Here are the conditions:

  1. Barcode Scanner will be used to scan the IDs of students using the arduino.

  2. Data will be stored in an SD card.

  3. A single VB program will be used to add students, see the database stored on the sd card, convert the database into excel file.

Please note that the system will only consist of the arduino. The software will be data management.