I’m testing out a stepper motor with a 100:1 reduction gear box attached.
The stepper is 42-H250B08, 24v, 0.8A, 200 steps/rev
The motor driver is a L298N breakout board
I’m using the standard “stepper_oneRevolution” example sketch just to test out the motors.
I changed the “stepsPerRevolution = 200” to “stepsPerRevolution = 20000” to account for the 100:1 reduction.
I also changed “myStepper.setSpeed(60);” to “myStepper.setSpeed(.6);” so as not to run the motor above it’s max rpm
Within 10 sec it had overheated the L298N and burned it out…
Any ideas why it would do this?
Code and Pics below
/*
Stepper Motor Control - one revolution
This program drives a unipolar or bipolar stepper motor.
The motor is attached to digital pins 8 - 11 of the Arduino.
The motor should revolve one revolution in one direction, then
one revolution in the other direction.
Created 11 Mar. 2007
Modified 30 Nov. 2009
by Tom Igoe
*/
#include <Stepper.h>
const int stepsPerRevolution = 20000; // change this to fit the number of steps per revolution
// for your motor
// initialize the stepper library on pins 8 through 11:
Stepper myStepper(stepsPerRevolution, 8, 9, 10, 11);
void setup() {
// set the speed at 60 rpm:
myStepper.setSpeed(.6);
// initialize the serial port:
Serial.begin(9600);
}
void loop() {
// step one revolution in one direction:
Serial.println("clockwise");
myStepper.step(stepsPerRevolution);
delay(500);
// step one revolution in the other direction:
Serial.println("counterclockwise");
myStepper.step(-stepsPerRevolution);
delay(500);
}
https://i.imgur.com/dOFtt6D.jpg