Hello,
I would like to see a STR710 header board like the LPC-H2214/LPC-H2294
Some of the main feature should be:
-
1MB (512x16) external SRAM perhaps 1xCY7C1061AV33 or 2xCY7C1049CV33
-
1MB (512x16) external FLASH
-
USB jack, USB with 48MHz external oscillator, like the original ST eval board.
(Here the USB from the CPU should be used)
-
16MHz external CPU clk
-
JTAG connector on the board
-
5V power jack
-
one or two leds
-
extension header for ALL uC ports, even the data AND address lines,
perhaps not all address lines up to A23 if it gets problems with the header.
But it would be nice if it is possible to map some external hardware in
the address space of the CPU.
- RESET circurit
Best regards,
Michael