Str710 +pp wiggler + write_image

Hi

I’ve just tried using

write_image and write_binary.

I’ve check the flash erases (and its not protected).

The problem i’m haveing is that write_binary works fine but write_image with either a hex or an elf file doesn’t:

flash write_image c:\Wireless\Wireless.elf

didn’t write section at 0x00000000, size 0x00000520

didn’t write section at 0x00001000, size 0x0000259c

didn’t write section at 0x00004000, size 0x0000a908

didn’t write section at 0x200024a8, size 0x00000004

or for the hex file:

wrote 0 byte from file c:\Wireless\Wireless.elf in 0s 0us (-1.#IND00 kb/s)

flash write_image c:\Wireless\Wireless.hex

didn’t write section at 0x00000000, size 0x00000520

didn’t write section at 0x00001000, size 0x0000259c

didn’t write section at 0x00004000, size 0x0000006c

didn’t write section at 0x00004100, size 0x00000018

didn’t write section at 0x00004200, size 0x00000018

didn’t write section at 0x00004300, size 0x00000018

didn’t write section at 0x00004400, size 0x00000060

didn’t write section at 0x00004800, size 0x000002a4

didn’t write section at 0x00005000, size 0x00009908

wrote 0 byte from file c:\Wireless\Wireless.hex in 5s 249798us (0.000000 kb/s)

Any ideas? [edit] this is using the v204

There have been some bug fixes to the hex and s19 reading code. i am updating svn today so try this newer version.

Regards

Spen

Thanks :slight_smile: