STUSB4500 Pwr Delivery Board isn't accepting any PDO

Hello!

I am having trouble getting my Sparkfun power delivery board STUSB4500 to accept any of the PDO options. I am trying to pull 9 volts from a portable li-ion battery that has power output options of 5V/3A, 9V/2A, and 12V/1.5A. Here are the NVM values I set stored on my power delivery board.

The PDO number is set to 3 so PDO3 should be attempted first which has a voltage set to 9V and a current set to 2A, which is what I want to pull. However, after I press the reset button on the power delivery board, disconnect it from my microcontroller (Arduino Nano R4), and connect it to my portable battery via a USB-A to USB-C cable, neither LED for PDO2 or PDO3 lights up and no voltage from GND and VSNK is read on my multimeter. Any advice is appreciated!!

Thank you!

The R4 is what holds the program that you’re uploading & saving; the Power Delivery Board isn’t a standalone device, it requires an MCU.

Can you power the R4 from the battery pack as well?

Thank you for your quick reply!

In the Power Delivery Board - USB-C (Qwiic) Hookup Guide page, there is an intro video where Rob Reynolds at minute 2:44 says “And, one of the nice things is once you programmed it (the power delivery board), you no longer need a microcontroller because the board can be self-contained.”

Then, not far below the video, there is a paragraph that says this:

“The STUSB4500 is a USB Type-C and power delivery controller IC for sink applications. The controller is able to negotiate a power delivery contract with a source (ie a power delivery wall wart or power adapter) without the need for an external microcontroller, although you will need a microcontroller to configure the board.”

Also, I hooked up the power delivery board to my battery and multimeter again today (without any wired connection to the Nano R4), and this time I got a 5V reading, but it drops down to 0 volts after about 30 seconds…

Thoughts?

Thanks!

Can you share a photo of the board’s connections?

Yes! Here it is.

Thanks! Also apologies for earlier, I was mistaken about how that board operates!

Does it work as expected if you plug the usb-A end into a 9v 2a (or more) wall wart? I’m wondering if the battery bank is also trying to do a negotiation behind it and tossing a wrench in the works

All good!

I tried what you suggested and connected the power delivery board to a computer charger that was plugged into a wall socket, and it worked! Thank you! The power delivery board negotiated as expected and I was able to pull 9V consistently! While I am glad that the power delivery board works, it seems like you are probably right in that it is unable to negotiate with a portable battery because the battery is also attempting some form of negotiation that confuses the power delivery board.

I know this is no longer in your scope, but I was wondering if you had any product or method suggestions to negotiate with a portable battery to pull 9V (given that the battery has a 9V output option). I am trying to create a warming device and want to push current through a metal wire to create heat. I want 9V and, if possible, to use a portable battery to provide that.

Thank you for all your help!

You could try a few things:

  1. usb-c to usb-c cable might be able to handle the handshaking (instead of the usb-a to usb-c being used)

  2. Try a PD Trigger/Decoy…I’d prefer one with solderable (or regular) jumpers to select the PD settings.

  3. If for some reason you can’t use usb-c as above you can also similarly try a QC Trigger (this just does the same negotiation on a QC/usb-a port). In either of these cases make sure you get a 9v capable one

Using a usb-c to usb-c cable worked! Thank you so much for all of your help. You are a life saver!