antdengineer:
This is my first time making a board in Eagle. I have 4 layers in this design and the two inner layers are Vdd and GND.
A four layer PCB is quite a bit more work and cost than
two layers. Why do you need four?
antdengineer:
The through-hole components have automatically been connected to the supply layers but I’m not sure how to connect surface mount components to the supply layers. Should I be using Vias?
Yes. If you turn off all layers except "Dimension" and
“Unrouted” (19 and 20) you should see air wires from
every SMD/SMT pad that has not been routed.
Use the “SHOW” tool (or type “SHOW ”) to
highlight your power and ground nets, one a time.
Manually route these and use vias to ‘staple’ the outer
layers to the inner planes.
A completed PCB will have zero (I mean none, not any,
not even little specs) on the Unrouted layer.
Turn off the grid and all other layers to check this very
closely. Just one of these will bring you a “green coaster”
instead of a PCB later!
antdengineer:
how can I draw an “Isolating Wire” around the edges of the board? What layer should this be?
This is probably something lost in translation...
I think it means that you should draw a poly around
your inner layers, and adjust the size to be inside the
physical PCB border. When fabbed the inner layers
will then have a non-metal perimeter clearance to
stop the layers form shorting together.
antdengineer:
And finally, does anyone have any general advice when using supply layers.
Avoid them if possible for low cost, easy to do
projects. (Unless you have no choice…)