Surveyor with Arduino Deci/Ardumato and Xbee Questions

I have a little OSBOT Surveyor which I am playing around with trying to get Xbee to control it. The stack is this: Arduino Deci/Ardumato/Sparkfun Xbee shield. I have a sketch that will control the Surveyor thru the serial connection. It is fairly generic and works well with the serial connection.

Here’s the thing. I have the Xbee’s blinking at each other but no movement. Weird since it runs with the USB cable just fine. The Xbee’s are doing there thing and the program is such that when I press a certain key it will go forward, another key backward, etc. You can see the Xbee transmitting and the receiving Xbee blink RX in response. So you assume the signal is passed and something is not getting from the Sparkfun Xbee shield to the Ardumoto to connect with the pins on the Decimmila. Anyone have experience with type of fault. Appreciate enlightement if you would be so kind.

Old hank 8)

Try hardwired connections instead of the XBees to start. Once that works then put the XBees back