Hello everyone,
I am facing a problem of not being able to send out information from xbee arduino shield to the xbee plugged into the laptop using the xbee dongle. Both xbee is not able to send and receive information from both sides. The program that i tried is the one that can be found in https://learn.sparkfun.com/tutorials/xb … ation-test.
Any help will be greatly appreciated.
The codes is as shown below.
/*****************************************************************
XBee_Serial_Passthrough.ino
Set up a software serial port to pass data between an XBee Shield
and the serial monitor.
Hardware Hookup:
The XBee Shield makes all of the connections you’ll need
between Arduino and XBee. If you have the shield make
sure the SWITCH IS IN THE “DLINE” POSITION. That will connect
the XBee’s DOUT and DIN pins to Arduino pins 2 and 3.
*****************************************************************/
// We’ll use SoftwareSerial to communicate with the XBee:
#include <SoftwareSerial.h>
// XBee’s DOUT (TX) is connected to pin 2 (Arduino’s Software RX)
// XBee’s DIN (RX) is connected to pin 3 (Arduino’s Software TX)
SoftwareSerial XBee(2, 3); // RX, TX
void setup()
{
// Set up both ports at 9600 baud. This value is most important
// for the XBee. Make sure the baud rate matches the config
// setting of your XBee.
XBee.begin(9600);
Serial.begin(9600);
}
void loop()
{
if (Serial.available())
{ // If data comes in from serial monitor, send it out to XBee
XBee.write(Serial.read());
}
if (XBee.available())
{ // If data comes in from XBee, send it out to serial monitor
Serial.write(XBee.read());
}
}