SX1509 internal pulldown failing

Looking for some help.
Connected a SX1509 to ESP32 running ESPhome.
I’ve selected “Pulldown: true” option for 4 of the GPIOs and initially they worked ok.
But over night these GPOI’s have lost the pull down resistor somehow.
The input/gpio is now floating 1.2vdc.
One of the gpio’s i had set to pullup but it now is floating too.

I’d sooner suspect fluctuating power or something…are you using a means-well supply? Can you put one on a big battery to run overnight to test with?

Hi
It’s a Poe device (Olimex ESP32-POE-ISO)
Yes something not right ill have to try a different power supply.
Thank you

Looks like a I2C problem only when i have two of the SX1509 connected.

Should i be removing one set of pullup resistors (SJ1) if im connecting two SX1509’s on the same bus?

thanks

Yes, you should only have one set of pull ups on the I2C bus at a time.