Hi All.
I am problem in my project with Telit Module to activate the GPRS from MCU UART.
I know the EasyGPRS AT Commands to Activate GPRS and send UDP Data. The strange issue is … when I an sending the AT Command manually by typing from PC Hyper-Terminal then all works. Module can send UDP Data to Server. But when I am sending exact same AT Commands from MCU UART then Module reply ERROR against AT#SGACT=1,1,“”,“”. But other AT Command reply is OK.
Below are my Command which I tried with Module Response (with Echo ON):
AT
OK
AT+CMEE=2
OK
AT&K0
OK
AT+CGDCONT=1,“IP”,“internet”,“0.0.0.0”,0,0
OK
AT#SGACT=1,1,“”,“”
+CME ERROR: activation failed
AT#SD=1,1,“31000”,“110.50.103.97”,0,0
+CME ERROR: operation not supported
HELLO
I tried the regular GPRS AT Command as well. Then same ERROR comes with AT#GPRS=1 Command.
Note: The problem only happens when I can sending the Command from MCU. Exact same Command working fine when sending from PC Hyper-Terminal … ![]()
Anyone can advise whats the issue?
Thanks in advance.
Regards.